(0)| 7/11/2018 6:43 PM | |
|
Posts: 24 Rating:
|
Hello: I´m having troubles trying to communicate a CP341 with an slave. Whats happening is that the TX LED does not flash at all. In the program I´m able to see that the message is been sent because the ¨Transference made with error¨ variable is been increment. In addition it shows the 830H error code. I´ve read that this specific error means that the time for receiving a response has elapsed, should not blink the TX led although? I´ve checked the pin out and its ok, also the configuration in boths slave and master is the same. Can you help me figure it out whats wrong? Any help will be great. Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/12/2018 10:35:47 AMNew subject after splitting |
|
Follow us on