(0)| 10/10/2018 2:19 PM | |
|
Joined: 4/28/2015 Last visit: 10/1/2025 Posts: 67 Rating:
|
Dear Experts I am using Simovert Masterdrive 6SE70 VC DC to AC for bridle roll application 11 kw. Presently ramp-down time in P 464 is 0.5 seconds. For modification I want to give this from PLC (S7-414) which I am calculating based on the line speed. (lets say it MW 500 in PLC). Now problem is that I could not find any Konnector (K...) which can transfer this value to P 464. I checked function block but it is showing P 464 only for rampdown time. Can somebody please help me finding how to achieve this. waiting for reply ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/10/2018 2:32:25 PMNew subject after splitting There is only one end of Knowledge, The beginning. |
|
Follow us on