(0)| 1/9/2019 5:10 AM | |
|
Posts: 7 Rating:
|
Hi all, I have a question related to this. By setting the input filters at 6.4ms does it mean that it can handle frequencies of approximately 156 Hz (1/6.4ms)?? In the past, I have had problems with adding a counter with the input frequency not exceeding 15 Hz. The same sensor outputs were used on 2 inputs (one as an HSC and another as a regular input). However, the counts were not the same. The regular input counter missed a few pulses from time to time. Using HSC is ofcourse an option but the problem is for 1214C there are 6 HSC (and there are a total of 14 DI). My application requires 12 counters at approximately 20Hz. (and no adding an additional input module is not an option here- BTW, do the input modules also support HSC?) Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/9/2019 7:58:47 AMNew subject after splitting |
|
Follow us on