(1)| 2/16/2019 6:41 PM | |
|
Posts: 51 Rating:
|
Just see the attachement, it does not need to be difficult. Keep in mind this is not a final setup just a idea. For the LDR's sensors they need to be installed on the panel looking at 90 degree from the panel witha small shade between LDR 1&2 also for LDR 3&4 also the setup LDR 1&2 are setup that they cover there movement.At a tresshold of 11 the motor will start to ballance back in ballance. At sun down (based on setup from the block) the setup will move back to start position. All positions are protected by limit switches. Extra you can include a storm position to move the panel horizontal ....... Attachmentsolar panel control.zip (334 Downloads) |
This contribution was helpful to
|
|
Follow us on