(0)| 3/12/2019 2:14 AM | |
|
Posts: 1 Rating:
|
Hi Dear I have built a SIMOCODE project in TIA portal V15.1 also its supported with SIMOCODE V15.1 software and SIMOCODE PRO V PN (3UF7011-1AB00-0) connected with Measuring Unit 63-630 Amps (3UF7114-1BA00-1) also I connect a load (4 AMPS ) for testing my project
after adding the items to TIA project : - The hardware article number appear in catalog information as a folding (3UF7 011-1A*00-0) (3UF7 114-1*A00-0) - the online status downloaded without any hardware and software error , voltage measuring reading the actual values but unfortunately SIMOCODE con't measure AMPS "" I select application /molded case circuit breaker and set current IS1 63 Amp after that I change IS1 to 6 amps with suitable transformation ratio but also the current still 0 after turn on the motor . could you please to help me in my case - is there any problem or effect with (*) witch appears in hardware catalog (no errors appear) ?? - My testing load is 4 amps it should be readable by (63-630 measuring unit with "IS1=63 A" ) or not ?? - finally if every thing is ok why the simocode could not measure any amps value?? please help me as much as you can
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/12/2019 6:45:49 AMNew subject after splitting |
|
Follow us on