(0)| 4/17/2019 1:00 PM | |
|
Posts: 1 Rating:
|
hi i have a siemens masterdrive DCmaster that is currently working fine via profibus, i took an upload of all parameters and downloaded them to another drive with the same confuguration (with drive monitor) and put that one in place. after download i checked the buss adress and it was 3, should be 20. i manually changed the adress to 20 and then checked for working, no faults or alarms but the motor isn't running as with the other masterdrive.Question, first is it normal that the adress isn't coppied with a download to drive? Second can there be a hardware conflict in the communication board and cud without giving a fault?
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/17/2019 2:38:03 PMNew subject after splitting |
|
Follow us on