(0)| 10/28/2008 7:45 AM | |
|
Joined: 9/27/2006 Last visit: 1/15/2026 Posts: 12481 Rating:
|
Hello saleem; I cannot be absolutely sure about an OP15c1, this model number does not bring any hits, from Siemns or the web. Here is a manual for the OP5 and OP15 operator panels that i have used. The software required to program them is Protool, it works with all Windows OS up to XP (depending on the version). Unfortunately the upload software is not integrated in Protool; it is called Prosave, and the backup it collects from operator panels is a compiled file that can only be downloaded to a similar panel (no modifications possible). And also unfortunately Prosave does not support OP15 units: From the Prosave Online help: ProSave can be used on the following operating units: · Text-based displays: TD 17, OP 7, OP 17, C7-633, and C7-634 · Graphic displays: OP 27, TP 27, OP 37, and TP 37 · All available Windows CE-based units |
Follow us on