(1)| 8/26/2019 7:25 PM | |
|
Posts: 49 Rating:
|
Hi, As I see, for internal CPU port it's neccesary to build the connection using TCON function, am I right? |
| 8/26/2019 7:59 PM | |
|
Joined: 4/7/2015 Last visit: 11/18/2025 Posts: 27 Rating:
|
Yes, you are right! According to manual: The MOD_CLI and MOD_SERV blocks called in the MODBUSPN FB use the TCON and TDISCON blocks from the standard library to establish or terminate connections between the CPU and the communication partner. You can find required information in the folow manual: SIMATIC SIMATIC Modbus/TCP Communication via the integrated PN interface of the CPU |
Last edited by: valrin at: 08/26/2019 20:01:46Last edited by: valrin at: 08/26/2019 20:04:33Last edited by: valrin at: 08/26/2019 20:13:15 |
|
| 8/26/2019 8:28 PM | |
|
Posts: 3093 Rating:
|
Hello, Here you can find an overview of the ModbusTCP libraries for S7-300/400. Regards, |
Last edited by: Kaulquappe at: 08/26/2019 22:59:06 |
|
| 8/26/2019 10:37 PM | |
|
Posts: 49 Rating:
|
Hi, I use a redundant system. As I see, the only thing to do for redundant is to define an extra connections in parameters block (I use Modbus Wizard for it). |
| 8/26/2019 10:46 PM | |
|
Posts: 49 Rating:
|
Thanks! As I see, for redundant system I need to use other functions. |
Follow us on