10/29/2019 4:56 PM | |
Joined: 4/28/2015 Last visit: 9/10/2025 Posts: 13 Rating:
|
I want to realize one path: spiral line, X axis and Y axis are moving cycle path, at the same time, Z is move slowly. one idea is X axis and Y axis move Synchronously with one virtual rotated axis named M axis. when M axis moving from 0 to 360 degree, X axis and Y axis's path is a cycle, and at same time ,Z axis move line Synchronously with M axis. the other idea is done in kinematic system , but we just have 4 instructions: movelinearAbsolute /movelinearRelative /movecircularAbsolute /movecircularRelative. In my opinion, one time we can just use one instruction, how can do realize my demands? if you have some ideas, please give me some directions, thank you. |
10/29/2019 8:17 PM | |
Joined: 5/6/2010 Last visit: 9/15/2025 Posts: 2031 Rating:
|
Hello, I don't know which PLC do you use, but SIMATIC S7-1500 S7-1500T Kinematics Functions V4.0 in TIA Portal V15 SIMATIC S7-1500T Getting Started with Kinematics regards |
10/31/2019 6:43 AM | |
Joined: 4/28/2015 Last visit: 9/10/2025 Posts: 13 Rating:
|
PLC is 1515T, that paper you gave to me I have read, but I still have the problem. thank you |
11/4/2019 8:38 AM | |
Joined: 4/28/2015 Last visit: 8/7/2025 Posts: 399 Rating:
|
Hello, did you notice these application examples or tool boxes yet? Maybe one of it will be helpful to solve your problem:
You will also find a selection of useful application examples, FAQs and manuals at the following topic page:
|
Follow us on