(0)| 4/1/2020 1:46 AM | |
|
Posts: 3 Rating:
|
Hi, I am having trouble with connecting to the internet on my IoT2040 when I set eth0 to a static IP address and turn eth1 off. I'm connected to a router that is using 4G (if that makes any difference), and when I SSH into the IoT at IP address 192.168.1.150 and try 'ping google.com', I just get
Now, following the instructions in this post, I create the resolv.conf file in /etc/ with the contents below and make it immutable. 192.168.1.1 is my routers IP Address.
Now I get this error:
I've also tried adding in namservers that are equal to my router's DNS with no luck. What's even more strange is that when I set eth1 to be DHCP and try obtain the IP address when plugged into X2P1, searching the topology of the network via my router's page, I am unable to see the IoT2040. Plugging back into X1P1, I see both the static IP and the DHCP address as different devices (see image). But I can SSH into both of them and they're both clearly the IoT2040. And now pinging google does work. To me this doesn't seem like the way it should work, am I wrong? I really just need to set a static IP address for the IoT2040 and have it successfully connect to the internet every time it boots. I appreciate any help. Cheers. |
Follow us on