(0)| 4/9/2020 7:25 PM | |
|
Posts: 1 Rating:
|
Hello gentlemen, the analog card 334-0SE -0AA0 broke and I got another card with the same features and pressed the blower with the wiring it had, but I see that the input which is 4-20 mA does not work while in the old one the damaged I see that it works from the monitor, the cable does not have a problem, my signal is coming, these cards are plug and the card and play, this news is repaired and I see in all its inputs to get the same price 7FFFH,Whatever the problem, thank you in advance. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/11/2020 09:31:42New subject after splitting |
|
Follow us on