(0)| 6/6/2020 12:58 PM | |
|
Joined: 1/13/2014 Last visit: 8/12/2024 Posts: 4 Rating:
|
Hi xMartin, Did you finally managed to install CPU 1507S F V20.8 on the IPC 427D?? Since a few days ago Im trying to upgrade a fully functional IPC 427D that was running firstly with WinAC RTX F 2010, and lately with CPU 1507S F V2.1, I ended up doing a clean installation IPC recovery DVD with WES7 sp1 x86 DiagBase V2.1 recommended windows KBs HD Graphics 4000 driver 15.33.35.4176 after installing the CPU 1507S F V20.8, reboot on windows+CPU 1507, when I try to power on the CPU from its panel I get this two oprions of Reset CPU or Terminate CPU, no matter which one I choose, I could never get the PLC powered on please do you have any comment to share? Thanks! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/08/2020 09:55:47New subject after splitting |
|
| 6/8/2020 9:56 AM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject Can't power on the PLC anymore is published within the conference SIMATIC S7-1500. Best regards,Jen_Moderator |
Follow us on