(1)| 2/1/2009 12:05 PM | |
|
Posts: 1690 Rating:
|
Hi Cheekyeng, for infos of NPN and PNP look at the internet and at the attached file.. At the LOGO! you can connect both. Then you must only use the corresponded I/O-pin in the circuit as activ "high" = "1"(PNP) OR as active "low" = "0"(NPN; = use it inverted). The LOGO! Memory Card (purple) provides storage for the circuit program. The LOGO! Battery Card provides battery backup of the real-time clock for up to two years. The LOGO! Memory/Battery cardprovides both circuit program storage and battery backup of the real-time clock. AttachmentNPN and NPN OPEN COLLECTOR electronic.pdf (1061 Downloads) |
This contribution was helpful to
|
|
Follow us on