(1)| 2/7/2021 8:50 PM | |||||
|
Posts: 35 Rating:
|
Hi again, you just triggered a memory. there are some settings called fixed frequency P041 to P044 on my drive you have to set P006 Frequency setpoint source select to setting 2 which is :- 2 =Fixed frequency or motor potentiometer. Fixed frequency is only selected if the value of at least one binary input (P051-P053) = 6, 17 or 18. and P051 to P053 are: - P051 DIN1, FF3 function select
mine default to P051 = 1, P052 = 1 and P053 = 6 (Fixed frequencies 1 - 3) im wondering if its these that are incorrect i tried changing these a while back but never got any of them to function sorry i copy and pasted and the table is out of alignment |
||||
| 2/8/2021 7:08 PM | |
|
Posts: 35 Rating:
|
Hi this is now resolved thanks to help from Tractor, see posting micro master speed change |
This contribution was helpful to
|
|
| 2/8/2021 7:23 PM | |
|
Posts: 35 Rating:
|
Hi, thanks for all your help too i have marked the action now |
This contribution was helpful to
|
|
Follow us on