10/26/2019 6:34 AM | |
Posts: 18 Rating: (0) |
Hello experts, I have tried to communicate the socomec Diris A40 with S7-400 dp master system. I did the all parameter setting from socomec Diris A40/A41 side. As per below link :- Also gsd was installed in hardware configuration .Also its signal strength checked through profibus tracer. I am facing the problem when insert module in hardware configuration.Because there are lots of module are showing in hardware catalog. Is there any document related to whats type module to be insert in hardware configuration. Configuration mismatched error is showing in module information. does someone has experience please share B/R Rama/tata ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/28/2019 11:27:47New subject after splitting |
|
11/26/2019 7:33 AM | |
Posts: 18 Rating: (0) |
Hello Daniel Chartier , Thanks for your support. I successfully communicated Diris A40 with S7-400 dp master system. I attached the screen shot of Diris A40 configuration which will help to other. B/R Rama/TATA AttachmentDIRISA40.pdf (556 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on