7/11/2013 5:25 AM | |
Joined: 7/8/2013 Last visit: 2/6/2022 Posts: 4 Rating:
|
Dear Members, I was working project S7300 with MD720-3 GSM/GPRS modem I have downloaded the Application Example for the same as available on http://support.automation.siemens.com/WW/view/en/25545680 and modified according to my existing CPU its317-2 PN/DP (317-2EK14-0A0B) and CP341 RS232C (341-1AH02-0AE0) and MD720-3 (720-3AA00) and I used SIM card PIN : 1234, short message center number :+66923010900 I am unable to get ready signal even after giving it a Initial request, I'm monitor in SCL code program keep sending step1 (ECHO OFF) to get OK from modem but, seem like the modem echo command back to CP please find in attachment file is my program kindly any one explain to me what my program issue Best Regard, B.Thanit
AttachmentMd720_ex.zip (833 Downloads) |
7/12/2013 5:39 AM | |
Joined: 7/8/2013 Last visit: 2/6/2022 Posts: 4 Rating:
|
> instance DB of the FB17 I forgot to compile right now was compiled no more red > I'm using S7/M7 RS232C (6ES7902-1AD00-0AA0) cable to connect to MD > the S LED keep flash slowly when it got command from PLC > I had tried to send AT command to MD with Hyper Terminal let's see in attachment file AttachmentCapture.zip (822 Downloads) |
7/12/2013 8:25 AM | |
Joined: 7/8/2013 Last visit: 2/6/2022 Posts: 4 Rating:
|
I have configured by AT command using Hyper Terminal already let's see in my attachment file Best Regard, Num
AttachmentCapture.zip (658 Downloads) |
7/16/2013 2:06 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Delete file with name "Language" from folder Global. |
9/12/2023 5:23 PM | |
Joined: 8/7/2019 Last visit: 9/28/2024 Posts: 1 Rating:
|
Hello, i have the same problem |