6/17/2009 1:21 PM | |
Posts: 18 Rating:
|
Hi https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&siteid=csius&aktprim=0&extranet=standard&viewreg=WW&objid=10803928&treeLang=en You can down load S110 parameter list manual from this link , in which you get detailed information about Profibus Communication. |
6/17/2009 3:20 PM | |
Posts: 65 Rating:
|
I already did that, but I do not get any further. Is it so that I also need to change the PLC program to send that NSOLL_A parameter? |
6/18/2009 11:50 AM | |
Posts: 65 Rating:
|
continuing... I already tried transfering to PQW 356 PQW 358 PQW 278 PQW 280 ... I tried them all, but still no luck What am I still missing? |
6/19/2009 3:57 PM | |
Posts: 107 Rating:
|
Hello! Since you want to send Speed setpoint over Profibus , I would recommend retaining the bit 10 in PLC. As far as switching ON/OFF of the drive is concerned, it can be done in 2 ways - 1. Go to the page "Control Logic" under Drives in Starter , under Control word sequence control bit 0 [ P840(0) ON/OFF1] you can select the binector which refers to the digital input you want to connect. 2. Go to Inputs / Outputs page under the controller , select the input you want to use, click on the connector, select the drive unit and from the pop up list select p840[0] I hope it's the same for S110. As far as S120 is concerned I am sure about it. Attachmentdrive_on_off.pdf (482 Downloads) |
Last edited by: Bhaskaran at: 6/19/2009 4:21 PMLast edited by: Bhaskaran at: 6/19/2009 4:18 PM |
|
6/23/2009 3:33 PM | |
Posts: 65 Rating:
|
Both solutions do not work.In both cases the textfield is greyed out. Probably because I selected Standard Telegram 1, PZD 2/2. |
6/23/2009 4:09 PM | |
Joined: 9/18/2006 Last visit: 5/31/2025 Posts: 596 Rating:
|
Hi. |
7/4/2009 11:47 AM | |
Posts: 65 Rating:
|
thx every1 for the explanation, I will tryit asap, but I don't know if it willbenext week... |
2/10/2010 11:48 AM | |
Posts: 65 Rating:
|
I'll try again as soon as I have the time again. |
4/12/2017 3:09 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4759 Rating:
|
New question published by Kanian10 is split to a separate thread with the subject S110, ready signal from my drive is not active. Best regards |
Follow us on