6/14/2014 8:59 AM | |
Posts: 3 Rating:
|
Hi! I'm using Simatic S7 300 (CPU315-2P), when its on RUN mode, SF and BUSF Leds are not blinking which means a Normal state BUT at the Simatic Panel in appears as attached (image.zip). What's happening? any advise? TQ Remy
AttachmentImage.zip (356 Downloads) |
6/14/2014 10:05 AM | |
Posts: 8946 Rating:
|
Ste39is right. If there is no problem with cable and plugs, it will be the easiest way to check program with PG or plug the Flash Card with actual program, if available. |
This contribution was helpful to
1 thankful Users |
6/14/2014 4:26 PM | |
Posts: 3 Rating:
|
Thanks all for the supports! There's been a power failure for more than 1 month and the CPU's battery run out. Didn't know how long the battery can lasted but I'm can confirm that the data blocks are missing. So what I did is just download to CPU thru PG using the last config blocks saved in my workstation and luckily the Simatic panel works as attached pic>Image2 (4). Unfortunately, some of the node's Profibus are inaccessible >Image2 (1,2,3), but it's working after I restart my workstation!! (does it relates at all??) 1) How can I save my current setting? 2) DP Master now looks weird as it shows red, yellow and green LED (on) as attached >Image2 (5) Why? 3) Our DP slave can now operates local and remote. AttachmentImage2.zip (345 Downloads) |
6/14/2014 5:39 PM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello RemyAdry, 1) Please have a look: What is the effect of the STEP 7 function "Copy RAM to ROM"? you need a MC (Big Blue Memory Card) or or as long as the battery lasts http://support.automation.siemens.com/WW/view/en/19102565 2) On the Masterdrive the three LED's are permanently ON or Blinking? ¨ During normal operation, all three LEDs repeatedly light up at the same time and for the same length of time (flashing)! ¨ If an LED is continuously on or off, this indicates an exceptional condition(parameterization phase or fault)! |
Last edited by: Ste39 at: 6/14/2014 5:52 PMLast edited by: Ste39 at: 6/14/2014 5:52 PMLast edited by: Ste39 at: 6/14/2014 5:44 PM |
|
This contribution was helpful to
1 thankful Users |
6/15/2014 2:45 AM | |
Posts: 3 Rating:
|
|
Follow us on