3/21/2024 8:36 AM | |
Joined: 4/18/2023 Last visit: 3/26/2024 Posts: 1 Rating: (0) |
FMT OBI Hello I have a setup with a redundant H-system CPU 1517H-3 PN. and two MTP1900 Unified panels. I use the default Diagnostic Overview. But there is no information available, the page is greyed out and shows nothing, like if it is not connected to a PLC. Shout it work on a H-system? Does it require a special setup? ------------------------------------------------------------------------------------------ |
Last edited by: U_30e8d004-be10-4e82-be2d-ba68b6147172 at: 03/21/2024 08:37:06Last edited by: Jen_Moderator at: 03/21/2024 11:34:32New subject after splitting |
|
Follow us on