9/3/2021 8:59 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051)
|
hi gcadenas, I´m afraid to say, that is not possible. You can check if the MAINT-LED is lit, but this can be also any other maintainence event. In my opinion it should be in possible with RT_INFO: Read out runtime statistics, but it isn´t. I also couldn´t find any other method to get the force state. But I also have to say, forcing should be nothing a user-program should run with, when there is no programmer working on it. When the programmer leaves the site forcing should be ended. hope this helps, regards, |
FCK WAR! |
|