(0)| 5/5/2021 9:17 AM | |
|
Posts: 2 Rating:
|
Good day. I am trying to configure a V90 drive for torque control using PROFinet.I use an S7-1500 controller. I select additional telegram 750 in the drive configuration, but it is not available when configuring the technology object. [snip] In the technology object, telegram 750 becomes selectable only when all modules are displayed. [snip] After downloading the project to the controller, the technological object throws a communication error. Please help to solve this problem.
AttachmentImages.zip (453 Downloads) |
Last edited by: Evgeniy_nf at: 05/05/2021 09:19:08Last edited by: Evgeniy_nf at: 05/05/2021 09:21:02Last edited by: Evgeniy_nf at: 05/05/2021 09:24:04Last edited by: Jen_Moderator at: 05/06/2021 06:58:14Added embedded image and other file as an attachment. |
|
Follow us on