(0)| 6/8/2021 10:50 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello Hazzem; In Step 5, BS 121 contains the average cycle time of te CPU, BS 122 poins to the Max. Cycle time, BS 123 shows the Min Cycle time. In Step 7, these values are part of the local data of OB1 and can be easily read out. You do not need your FC1 for this purpose in a step 7 program. See our friend Umencho's answer here: The screenshot below is taken from the System and Standard Functions for S7300/400 CPUs. https://support.industry.siemens.com/cs/ww/en/view/109751826 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 06/08/2021 22:51:32Last edited by: dchartier at: 06/08/2021 23:02:00 |
|
| 6/9/2021 1:07 AM | |
|
Posts: 33 Rating:
|
Thanks dchartier, it's so clear and it works. |
Follow us on