7/9/2021 6:12 AM | |
Joined: 5/3/2018 Last visit: 2/15/2025 Posts: 56 Rating:
|
Hello Guys Could anyone soon reply on the above query I have posted. Thanks |
7/9/2021 10:16 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi Raghu Kodi, When you use redundant IOs, It would also make sense to have the IMs redundant. There is only one programm, and also only one address for the IOs. But the program is running on two PLCs. When one PLC or IM or IO is faulty the back-up deivce can take over. I guess you need more information, than we can deliver here in the forum, because these are very basic questions regarding H.controllers. Have a look into the manual: SIMATIC S7-1500 S7-1500R/H redundant systemIf you don´t have a S7-1500H, use the search button for a more relevant manual. hope this helps, regards, |
FCK WAR! |
|
7/9/2021 3:49 PM | |
Joined: 9/27/2006 Last visit: 9/13/2025 Posts: 12408 Rating:
|
Hello Raghu; MopSO4 is quite right, your requirements at the level of interface modules conected to a redundant controller system will depend on the type of redundant controller and network topology used in your application. The sceenshot below used these 2 documents to compare a redundant S7-400H system, with redundant ET 200M interfaces over Profibus, and a redundant S7-1500 R/H sytem using a Profinet ring to connect to ET 200SP remote I/O racks (non-redundant interfaces): - Configuration of Redundant I/O Modules in SIMATIC PCS 7 (S7-400H) https://support.industry.siemens.com/cs/es/en/view/28430682 - Connection of redundant I/O devices to S7-1500 https://support.industry.siemens.com/cs/us/en/view/109767576 If you feel we can offer more information, pray tell us more about your system. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 07/09/2021 15:52:20 |
|
Follow us on