8/2/2021 5:20 AM | |
Joined: 5/3/2018 Last visit: 2/15/2025 Posts: 56 Rating:
|
Hello Everyone, Can any help me solve the above query. Thanks |
8/2/2021 10:26 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi, DP/PA Link connection with 2 CPUsIt is exact the same question. The only difference is that it is an other DP-slave. As long as the addresses and the configarion of the slaves are the same in each system it should work. so the answer was already given. Are there any problems on this? Have you tried it? regards, |
FCK WAR! |
|
This contribution was helpful to
1 thankful Users |
8/2/2021 10:56 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject DP/PA Link connection with 2 CPUs is published within the conference Decentral Peripherie. Jen_Moderator |
Follow us on