2/3/2022 11:50 AM | |
Joined: 9/27/2006 Last visit: 9/2/2025 Posts: 12397 Rating:
|
Hello Rodrigo; You are right that the Profibus-DP interface of your PLCs cannot be transformed into a Profibus-PA slave interface. The physical layer and the protocol are too different. If you want to go onto details, open the Downloads link at Profibus.com, Profibus International provides official documentation on both protocols. An interesting detail: one of the reasons Profibus-PA can have such extended segment lengths is because the transmission layer MBP (Manchester-coded, bus powered) operates at relatively low speeds, 31,75 kb in the PA segment. 45,45 kb in the DP/PA coupler. On Profibus-DP networks, as soon as you operate at 187,5 kb or less, your segments can run up to 1000m, before the first repeater is required. And if you want star or tree topologies, along with long spur lines in a Profibus-DP environment, Procentec has been proposing Profihub modules for years: https://procentec.com/products/profihub/ So there are ways to emulate a Profibus-PA topology with Profibus-DP networks. Hope this helps, |
2/3/2022 5:40 PM | |
Joined: 9/27/2006 Last visit: 9/2/2025 Posts: 12397 Rating:
|
Hello Rodrigo; My experience with Profibus up to now made me understand that chaning a Profibus-DP slave ro a PA device required a change of electronics, namely the ASIC chip. I believed different ASIC chips were required for a Profibus-DP and Profibus-PA slave. So it would require changing out the circuit board with the correct ASIC to switch a DP slvae to a PA device. Now however I have found that Procentec (an other manufacturers, such as Siemens) offers a SPCA4 or SPCA4-2 DP/PA Protocol ASIC that can be used to implement either a DP slave or a PA device. Note that the microcontroller attached to the ASIC shold be programmed according to the protocol selected, so it would require extensive reprogramming, and would still not be an easy task to transform a DP slave into a PA device. "It has to be operated with a processor and heavy protocol software." https://www.profibus.com/products/product-finder/spc4-dppa-protocol-asic Regards, Danieel Chartier |
Last edited by: dchartier at: 02/03/2022 17:42:47Last edited by: dchartier at: 02/03/2022 19:12:41Last edited by: dchartier at: 02/04/2022 15:52:45 |
|
This contribution was helpful to
1 thankful Users |
Follow us on