2/3/2022 6:46 AM | |
Joined: 12/18/2014 Last visit: 9/12/2025 Posts: 35955 Rating:
|
Use the function "Acknowledge message" in the message text. This display the message text till you acknowledge the message with the OK button of the LOGO! and the failure isn't there ... AttachmentMessage_text_acknowlegde_0BA8.Standard.zip (260 Downloads) |
This contribution was helpful to
1 thankful Users |
2/4/2022 12:04 AM | |
Joined: 6/11/2019 Last visit: 9/10/2025 Posts: 2628 Rating:
|
With the Logo you do not have the possibility to access and save the current time parameters. In order to get to it, you either have to program an auxiliary clock, with all its limitations and disadvantages, or get the time from another device (e.g. another logo) (there is already a topic about this in the German part of the forum). If you then have these time values, you write them to a self-programmed bucket chain memory when you trigger them. The values of the individual memory cells can then be shown there in the text display. Kind regards Ella_68 |
Follow us on