2/24/2022 3:41 PM | |
Joined: 6/12/2012 Last visit: 6/25/2025 Posts: 165 Rating:
|
I used XWorks 6.0 to program a PXC50-E.D. and created a Desigo Compact v5.0 Project, but it was necessary to update it to version 6.3, as we needed more than 50 DataPoints and this was only possible if we upgraded. I made the update, replacing the PLC in the Project Manager, but now when importing to Desigo it gives the error that you can see in the attachment. I also tried to copy the DataPoints structure in the CFC to a new PLC, but I still have the same error. Do I need to update Desigo? If yes, how can I update? AttachmentDesigo erro on importr.zip (380 Downloads) |
Thanks, |
|
2/25/2022 7:46 PM | |
Posts: 23 Rating:
|
Hello, Have you installed Quality Update? QU1 is minimum to make this working. Here is QU2: Desigo CC V5.0: products family Quality Update 2 - ID: 109806259 - Industry Support Siemens BR |
This contribution was helpful to
1 thankful Users |
2/26/2022 12:25 PM | |
Joined: 6/12/2012 Last visit: 6/25/2025 Posts: 165 Rating:
|
Thanks Khazzir. |
Thanks, |
|
Follow us on