(0)| 3/2/2022 6:05 PM | |
|
Posts: 257 Rating:
|
The Mobile Panels of 177 and 277 series are currently being discontinued. So are their system components such as connection boxes. See discontinuation announcement This phase-out was already declared on 01.10.2016, which heralded the phase-out period of a planned 10 years. This means that the use of these units is not recommended for new installations. Nevertheless, the units can still be ordered. This is still the case in the case of this junction box, although this is due to change to product deletion on 01.10.2021, so that new parts can no longer be obtained and only replacement units will be made available. The successors of the devices are already deposited in the discontinuation declaration. The 2nd generation Mobile Panels with their system components are recommended for this purpose. These are to be connected to the connection boxes exclusively via PROFINET. Best regards, SIMATIC International Technical Support Hub |
Follow us on