3/15/2022 1:48 PM | |
Joined: 11/11/2017 Last visit: 7/10/2025 Posts: 190 Rating:
|
can soemone take a look at this little UDF i have made. the start signal turns on a delay timer then after the delay it operates a foward output then a reverse output but when i press reset it does not do anything and i cant see why. even if the input start is on, i still need it to reset Thanks AttachmentFWDREV.zip (346 Downloads) |
Follow us on