(0)| 12/15/2020 5:03 PM | |
|
Joined: 6/28/2019 Last visit: 9/12/2025 Posts: 13 Rating:
|
Hi, I have a problem with displaying the logged alarms in my alarm view (I'm not even quite sure there get logged). I have about 20 discreet alarms, all linked with trigger bits, all working fine in alarm view when Alarm source = pending alarms. Now I've created the new alarm log, as the storage medium I've selected SD-X51, card is placed in the correct slot in HMI, on the screen ticked 'Activate data memory card slot', log file is assigned to the alarm class I am using. I've placed new alarm control, selected alarm source = logged alarms (tried logged alarms updated too), downloaded to HMI but no alarms are shown apart from active ones (which are effectively pending). When I press 'show logged alarms' or 'show and update logged alarms' buttons I see blank table.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/16/2020 10:22:32New subject after splitting |
|
Follow us on