8/24/2011 10:17 PM | |
Joined: 7/18/2011 Last visit: 4/11/2025 Posts: 521 Rating:
|
Hello Ali KK Take a look at this tread https://www.automation.siemens.com/tf/WW/en/Posts/16888 Kind regards BV |
4/22/2022 3:10 PM | |
Joined: 12/14/2021 Last visit: 9/22/2022 Posts: 1 Rating:
|
But the link you are referring to is for 153 and not 157. Is it still the same answer/procedure? |
4/22/2022 4:57 PM | |
Joined: 9/27/2006 Last visit: 9/2/2025 Posts: 12396 Rating:
|
Hello; A FDC157-0 (6ES7157-0AC85-0XA0, for example) is a field device coupler for Profibus-PA. If you use a IM 153 (6ES67153-2BA70-0XB0, for example) with up to 4 FDC157 on its rack you are building a DP/PA Link. There are diffrences on how you use and configure a DP/PA coupler (standalone) and a DP/PA link, this is explained in the following document: - How do you set up the DP/PA link and how do you configure the DP/PA link and DP/PA coupler? https://support.industry.siemens.com/cs/ww/en/view/51678187 Hope this helps, |
Last edited by: dchartier at: 04/22/2022 20:25:20 |
|
Follow us on