4/27/2022 3:36 AM | |
Joined: 10/7/2005 Last visit: 9/3/2025 Posts: 3049 Rating:
|
Hi Mohammad it is not only possible, but rather highly likely and FAQ Entry ID:14628680 has the relevant info on this (and note too its mentioning of Step 7 inbuilt help on this subject).
Only the obvious one that you have other Blocks where you use AR1 in the logic. Long story short, if you want to re-use AR1 contents from one block call to the next, you need to save AR1 at the end of the block call and load it again at the start of the next. |
Cheers |
|
This contribution was helpful to
1 thankful Users |
4/27/2022 2:59 PM | |
Joined: 9/14/2021 Last visit: 1/31/2023 Posts: 99 Rating:
|
I would be very happy if you tell me what the hell is this AUF DI ... I googled that but nothing find!! I think DI means "Instance DataBlock", yea?! |
Just with a floral skirt♥♣, and nothing else |
|
Follow us on