7/7/2022 12:21 PM | |
Joined: 6/13/2022 Last visit: 3/14/2023 Posts: 5 Rating:
|
Hi. I try to used one old CPU1212C (alone) and have one error (blinking red). I have updgraded firmware without sucess and have diagnostic message below.: ********************************************************************************** CPU error: New I/O access error during process image update During the system process image update, a new error has occurred leading to the adaptation of the process image update list. ********************************************************************************** I have send diagnostic rapport. Is-it definitively out or is threr somethings to do to solve this ? AttachmentDiagnostics 7_7_2022.txt (564 Downloads) |
Follow us on