8/29/2022 2:48 PM | |
Joined: 1/15/2018 Last visit: 11/14/2024 Posts: 6 Rating:
|
Hello, I have a similar problem but more specific. I want to prevent a SIMOTON D from going to stop when it detects a hardware module problem. In normal PLC or Sinumerik I always used OB122, is there a similar function designed for simotion (ours is used with TIA 15.1)? The problem occurs only when we are powering on the machine. Is there a configuration that I can enable to prevent it from going to stop with hardware fault or a Function/program that does it in SIMOTION? Best regards Bronek ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 08/31/2022 10:29:44New subject after splitting |
|
8/31/2022 7:05 AM | |
Joined: 5/12/2006 Last visit: 9/15/2025 Posts: 22710 Rating:
|
do you have a diagnostic buffer with the reason for stop? |
8/31/2022 2:53 PM | |
Joined: 10/11/2006 Last visit: 9/15/2025 Posts: 6040 Rating:
|
please find information about your enquiry in attached document
AttachmentPeripheralFault.pdf (769 Downloads) |
With best regards, |
|
Follow us on