11/19/2022 11:57 AM | |
Joined: 1/11/2019 Last visit: 8/14/2025 Posts: 899 Rating:
|
Hello Cristian, For the integration of frequency-controlled drives, Siemens offers a modern channel block, "FbDrive", which is part of the PCS 7 Advanced Process Library (APL). The channel block makes it possible to integrate drives in PCS 7 that support standard telegram types 1 or 20 and which can be recognized by the driver generator Kindly go through the below link to know the usage of FbDrive block and using the same for configuration Configuration of Frequency Converters with the APL Channel Block "FbDrive" in SIMATIC PCS 7 |
This contribution was helpful to
1 thankful Users |
Follow us on