11/16/2022 11:44 AM | |
Joined: 5/18/2021 Last visit: 3/14/2024 Posts: 12 Rating:
|
When I'm adding some new Control strategies in SFC type , I'm unable to get some of the new strategies added in Simatic batch.Please guide me on this Software version: PCS7 9.0 SP3 With Simatic BATCH V9.0 SP1 Updt5 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/16/2022 13:03:26New subject after splitting |
|
11/16/2022 4:24 PM | |
Joined: 3/14/2008 Last visit: 9/4/2025 Posts: 2216 Rating:
|
Hi, Make sure you enable the new control strategies in the properties of the SFC type in the master library/project library. There is a special dialog in the properties. Go to the SFC type, right click and open properties and you can find it there. |
If I could help you, you can use the RATE button. Thank you. |
|
11/17/2022 5:46 AM | |
Joined: 5/18/2021 Last visit: 3/14/2024 Posts: 12 Rating:
|
Even after selecting the newly added CS in the SFC Type properties check boxes, after an entire compile, load and Batch entire download(Generate, Propagate, Merge) the new strategies weren't listing in the list of Control Strategies in the Batch Instances folder of that particular EQM .Please find the attachment document with the necessary screenshots.
AttachmentCS SCREENSHOTS.docx (372 Downloads) |
Follow us on