12/13/2022 1:23 PM | |
Joined: 9/12/2019 Last visit: 8/18/2025 Posts: 17 Rating:
|
Good morning everyone. She had a doubt. In the old Siemens screens I configured the variables as Cyclic during operation, and with 60-second cycles and the screens were in charge of filling in temperature data. If the voltage went down or a modification was made, the values would be lost, but this solution served both me and the clients. Now with the new screens I don't see a way to replicate the same operation. How do I set the temperatures to be saved on screen without having to buy a usb or SD card by default? I would appreciate if you could help me. All the best, Samuel
AttachmentSiemensAyuda.pdf (415 Downloads) |
Last edited by: SamusEG at: 12/13/2022 16:25:35Last edited by: SamusEG at: 12/13/2022 16:26:03 |
|
12/14/2022 1:47 PM | |
Joined: 9/12/2019 Last visit: 8/18/2025 Posts: 17 Rating:
|
No, i use a real HMI, but no save nothing values for the Charts of Temperature. |
Follow us on