12/25/2022 3:52 AM | |
Joined: 11/14/2022 Last visit: 7/10/2023 Posts: 21 Rating:
|
Hello, everyone! I have a problem about exporting the status values of the global variables form SCOUT TIA online. (SCOUT TIA 5.4.3.0 in TIA V17) I want to export the global variables of a unit in the ".csv" format. My operation is to right click the whole symbol browser and click "save as", then I can export the global variables in the ".csv" format. However, the data set in the file exported is not completed and exists many "---" instead. Only several status values I unfolded and browsed can be successfully exported and displayed. There is a large size of array, so it is impossible to browse every element in that array. Can you give me some advice, please? Also, exporting large array from the symbol browser exist performance conflicts in my PC. If I export several large arrays one time, the SCOUT TIA may lose response. So, any other method to export global variable data will be welcomed! Thanks! AttachmentThe status values.zip (787 Downloads) |
Follow us on