(0)| 1/12/2023 9:09 AM | |
|
Posts: 41 Rating:
|
I would like to try to configure a MP370 panel as OPC server. I am follwing this example: What options are there in WinCC flexible for using a Multi Panel or Mobile Panel a... - ID: 22701694 - Industry Support Siemens I have install the example application in the panel and from an OPC explorer, in this case Itegration Objects OPC Data Access, I try connect. This is the dialog to connect to a new server: But I get an error: the RPC server is not available. Really I have tried with all the OPC servers name, but no one of the works. So perhaps it is because I am not using the correct OPC server name. How could I find the name of the server? The panel works as OPC XML server, so it is not needed to configure COM services like in the case of Windows. Is this correct? |
Last edited by: Jen_Moderator at: 01/12/2023 12:55:37Link optimized. |
|
| 1/12/2023 1:25 PM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject How to configura the OPC server in a MP370 panel? is published within the conference SIMATIC WinCC flexible. Jen_Moderator |
Follow us on