(0)| 1/21/2023 10:48 AM | |
|
Posts: 41 Rating:
|
I am trying to configure a shared folder in a PC with windows 11 to store csv files from a MP370 panel. To test if I can access to the shared folder, in the panel, in the file explorer, I enter in the network folder and in the address I write the path of the shared folder: \\PlcServer\csv At this point, I am prompted for the credentials. I set the user that I have created in the PC and I set the password. I check the checkbox to update the default credentials. But it seems it doesn't save it, because I am promted one and another time. it is similar to the problem that this used had: https://support.industry.siemens.com/forum/es/en/posts/logon-to-network-server/32063 Also, I am following this guide: https://support.industry.siemens.com/cs/de/en/view/13336639 Anyway, my problem is not configurating the PC, I enabled SMB 1.0, I create a user in the PC called SIemens that has permissions to modify in the sharing options and it has modify permissions in the security options of the folder. Also de panel can find the folder. The problem is when I am prompted to set the credentials, that are not accepted for some reason.
EDIT: in the server, in the events viewer, if I see the events of the SMB server, I see this error:
So it iseems that there is a problem when the panel tries to authenticate. |
Last edited by: GTSAGarcia at: 01/21/2023 10:49:45Last edited by: GTSAGarcia at: 01/21/2023 11:35:45Last edited by: Jen_Moderator at: 01/23/2023 10:34:18Link optimized. |
|
Follow us on