(1)| 1/26/2023 8:38 PM | |
|
Joined: 3/3/2021 Last visit: 3/5/2025 Posts: 21 Rating:
|
Thsnk you for reply .. I want this change time with LOGO .. |
| 1/26/2023 10:41 PM | |
|
Joined: 6/11/2019 Last visit: 1/18/2026 Posts: 2729 Rating:
|
Hello ALMOHARG, I can think of two options. With one, the input is evaluated and the display shows whether you are outside the input window. If this is the case, the triggering of the time relay is interrupted (sample 1). With the other option, the time is converted via inputs (e.g. logo button UP and Down). This variant can be supplemented with a "Push and Hold" (Sample 2). In both variants, the time is entered on the time basis of the delay module (e.g. 1 minute and 30 seconds are then 90 seconds) Kind regards Ella_68 (translated with Google) AttachmentSchaltplan1.zip (475 Downloads) |
This contribution was helpful to
|
|
| 1/27/2023 2:50 AM | |
|
Joined: 12/18/2014 Last visit: 1/18/2026 Posts: 36482 Rating:
|
Here's another possible solution.
AttachmentStore_only_accepted_values_0BA8.Standard.zip (495 Downloads) |
| 1/27/2023 7:01 PM | |
|
Joined: 12/18/2014 Last visit: 1/18/2026 Posts: 36482 Rating:
|
Yes, you're right. But it is not a small, but a big bug. Here's the corrected version. AttachmentStore_only_accepted_values_0BA8.Standard_V2.zip (458 Downloads) |
This contribution was helpful to
|
|
Follow us on