2/23/2023 12:55 PM | |
Joined: 4/7/2012 Last visit: 9/14/2025 Posts: 132 Rating:
|
Hallo. We are looking to upgrade a machine based on s7-400 to s7-1500. in the original Hardware configuration I have a IM 153-2 interface with some serial comunication cards. I searchet the GSD file and install it on Tia portal PROFIBUS GSD files : ET 200M - ID: 113498 - Industry Support Siemens but after installation only few IM153 are available, Can I setup the Hardware configuration with different module code ? or I do have to replace that IM? Thanks |
Last edited by: Jen_Moderator at: 02/24/2023 07:20:50Link optimized. |
|
2/24/2023 6:06 AM | |
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Hi,
There are different GSD files available, please choose the file for your interface modules. Some of these files contains "placeholders" like "6ES7 153-2BA*1-0XB0" This file could be used for all interface modules for which the article number is only different at the "*" mark. Otherwhise, please tell us the exact article number of the interface module. regards sancruz |
Feedback appreciated, please rate |
|
2/24/2023 7:21 AM | |
Joined: 4/7/2012 Last visit: 9/14/2025 Posts: 132 Rating:
|
Finally I installed the GSD and I can drag & drop the IM in my project (I have to choose it from "other devices") BUT the sub modules catalogue it is incomplete , so unfortunately it is not available the CP340.... I think I've to migrate to an IM available in the TIA catalogue. Thanks anyway. |
Follow us on