4/13/2023 11:49 PM | |
Joined: 1/1/2023 Last visit: 4/14/2023 Posts: 3 Rating:
|
Greetings, I am new to Siemens Logo PLCs and I need your assistance. I have a project file that I want to upload to my Logo PLC (0BA5), but it says it is incompatible because it was created with the default settings in Hardware type (LOGO! 8.3). How can I change the hardware type so that I can upload the program to my PLC without redoing the whole project? I have attached the program and the hardware type options for your reference. Appreciate your help AttachmentLOGOBooster_v2_2_10.zip (373 Downloads) |
4/14/2023 2:04 AM | |
Joined: 6/11/2019 Last visit: 8/31/2025 Posts: 2623 Rating:
|
But you can also copy the program into a new one that was previously set to a 0BA5. But first all text modules must be deleted and then recreated! It should be noted that you only have 10 text blocks available with the Logo 5, so that you have to do without some (I did the first step. But you have to insert the text modules yourself). greeting Ella_68 AttachmentBooster v2_2_10_o_D.zip (379 Downloads) |
4/14/2023 11:10 AM | |
Joined: 1/1/2023 Last visit: 4/14/2023 Posts: 3 Rating:
|
Thanks a lot for your help. Problem is solved, by removing text boxes and re-creating them in Logic 5 program. |
Follow us on