(0)| 4/13/2023 5:38 PM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hi, Are you using hardware modules that are released for PCS7 V9.1? Using the Released Modules manual. If they are not present, this could result in problems you have right now. |
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
| 4/14/2023 10:18 AM | |
|
Joined: 8/1/2019 Last visit: 12/8/2025 Posts: 304 Rating:
|
how can i find out if the attached hardware in the image are released for v9.1 sp2? |
| 4/14/2023 10:26 AM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hi, You need the slave MLFB number, now you have the IO module so one level above. A good rule is to check if the slave is listed in the PCS7_V91 catalog. You can also select the Standard catalog which shows all modules (even not released for PCS7).
|
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on