(0)| 5/19/2023 5:10 AM | |
|
Joined: 12/1/2012 Last visit: 1/13/2026 Posts: 135 Rating:
|
Dear All , Facing Problem of cannot create OCM attributes in Simatic Manager 5.7 . |
| 5/19/2023 7:17 AM | |
|
Joined: 5/6/2022 Last visit: 1/15/2026 Posts: 589 Rating:
|
Hi CP_S7, In relation to this error, tell you that the following options should be examined: -> CFC only supports STEP7 V5.7 as of CFC V9.0.5.4. In addition, the S7-PM V5.7 product and license are required. With S7-PM and the current CFC version it works without any problems. Otherwise, surely the project will surely have to be fixed from the development of Siemens. Hope this information can be useful. |
Last edited by: ElonksuM_SN_BN at: 05/19/2023 07:18:23If this Information really helps, you could use the Rate function |
|
Follow us on