(0)| 7/17/2023 10:07 AM | |
|
Joined: 5/19/2023 Last visit: 1/14/2026 Posts: 1 Rating:
|
Hi, I've got a problem with torque limiting S110 drive. Its configured as speed control. I'm changing p1511 Additional Torque 1 and its scaling is set to 100%. The drive runs at full speed, even though the torque is over the limit. I'm surely missing something obvious... Please see the attached Starter project. All 5 drives are configured the same.Here's screenshot of Torque setpoint - Additional torques page from Starter. You can see that actual torque is over the limit. @EDIT: I've found the answer: I didn't set bit 14 of STW1: Change over closed-loop speed/torque control. Attachmentflex_MWN.zip (487 Downloads) |
Last edited by: U_d3a74573-0b9a-46f7-8483-8be260465688 at: 07/17/2023 10:10:16Last edited by: U_d3a74573-0b9a-46f7-8483-8be260465688 at: 07/17/2023 10:42:17Last edited by: Jen_Moderator at: 07/18/2023 07:21:01Link removed and all files attached as .zip file. |
|
This contribution was helpful to
|
|
Follow us on