(0)| 10/19/2023 7:45 AM | |
|
Joined: 8/3/2009 Last visit: 1/20/2026 Posts: 16653 Rating:
|
Hello Wayse2 the basic FAQ: LINK In the HMI project you have a HMI connection in the connection editor. this has a logical access point (usually its S7ONLINE but you could also use another one). In teh PGPC interface you have to set the used Access point to an internal communication (PLCSim) or to a networkcard to get access to a real PLC or to a PLC Sim Advanced on another PC. You could also run multible Accesspoints in PGPC interface parallel. Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on