11/12/2023 9:23 PM | |
Joined: 10/11/2023 Last visit: 5/9/2025 Posts: 25 Rating:
|
Hey I've same problem too! in my case I have cartesian portal robot with 5 axes ( X1,X2(slave), Y, Z1,Z2(Slave)). As hardware CU320 2PN DP and all of encoders are absolute encoders and I've also 3 external encoders via SMC30 sensör modul transmit data to control unit!. I'm homing every time when power off and on or when cpu stop and start. How I can keep the home positions ?. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/13/2023 11:37:30New subject after splitting |
|
11/13/2023 11:38 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject Home Position loss in CU320 Control Unit is published within the conference SINAMICS S. Jen_Moderator |
Follow us on