8/5/2024 7:26 AM | |
Joined: 10/31/2005 Last visit: 4/22/2025 Posts: 366 Rating:
|
I also have this same error, however the project is TIA v18, loaded to PLCSIM Adv v18, so there is no real HW. What is specific here is the fact that when initially loaded, for a firs 2-3 min, everything is green and then suddenly this error appears. The only change in the diagnostic buffer is time sync error, but I doubt that is the case. I have read that deleting a connection in topology view could fix a problem, but actually there are two connections, one is to PN Coupler, while other goes to SCALANCE switch. I have added attachment with a compiled screenshots. In the hierarchy there is no other components that are red, so I guess the solution could be to delete the connection in Topology view, but I'm not sure which one and what effect that could have when this project is later downloaded to the real PLC. Do you have any advice? Thank you! Edit: Deleting connection from the CPU to the SCALANCE switch didn't help. When loaded, first everything is green for a certain period of time, then the error reappears. ------------------------------------------------------------------------------------------ |
Last edited by: Pandiani at: 08/05/2024 07:39:03Last edited by: Moderator_Lan at: 08/05/2024 11:31:56New subject after splitting |
|
Follow us on