8/7/2024 10:50 AM | |
Joined: 5/6/2022 Last visit: 7/10/2025 Posts: 589 Rating:
|
Hi AutoGen_8205947, What you are experiencing is a crash of the TIA Portal software. In this case, the first thing to do is to check a number of points: - Capture the exact version of Windows that you have installed. - Capture the versions that you have installed in the TIA Portal (Help > Installed software) - Does the crash occur with any project or just with this one? If after checking these points everything is correct, I would recommend that you contact technical support. Best regards!
|
If this Information really helps, you could use the Rate function |
|
8/7/2024 11:45 AM | |
Posts: 7 Rating:
|
|
8/7/2024 12:04 PM | |
Joined: 5/6/2022 Last visit: 7/10/2025 Posts: 589 Rating:
|
Hi AutoGen_8205947, I have been checking the compatibility and the problem is that the TIA Portal V16 Update 1 version is not compatible with the Windows 11 Enterprise version. In this case, I recommend you to upgrade to the latest version of TIA Portal V16 Update 7. I share with you the download link below: When you install it you should not crash the software. Best regards! *I forgot adding you the compatibility list* AttachmentMicrosoft-Windows-11_es_2024-07-24.xlsx (440 Downloads) |
Last edited by: ElonksuM_SN_BN at: 08/07/2024 12:05:56Last edited by: ElonksuM_SN_BN at: 08/07/2024 12:06:40If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
5 thankful Users |
Follow us on